| 02/08/2010 - Revolvo Slashes Lead Times For Large Bearings By 400% With Nearly £1M Investment In Two New GER Vertical Grinding Machines |
Revolvo's almost £1m investment in two new GER CNC grinding machines has improved its throughput of large solid bearings (over 500mm) by over 400%, cutting the lead times currently offered by bearing majors, which average 18-24 month's, to around 24-week's.
The two new GER vertical gri...More...
|
| 19/07/2010 - Energy Saving Rebuild for Industrial Tyre Shredder |
ERIKS UK has recently applied its engineering know-how to the re-manufacture of a tyre shredder used at one of the UK's largest tyre recycling centres. ERIKS' ability to provide repair services in addition to OEM component specification and supply has allowed it to provide a full service solution for machine rebuilding tha...More...
|
| 01/07/2010 - Tough seals meet face-to-face |
A new range of low-speed, metal-faced rotary seals.
Pioneer Weston has combined two areas of ERIKS Group expertise to develop a new range of rotary seals for arduous applications.
A new range of metal-faced seals from Pioneer Weston draws on 60+ years of experience designing, developing and manufactur...More...
|
| 21/05/2010 - Putting the seal on food safety |
 ERIKS is setting the benchmark for food safety with blanket (EC 1935) extraction testing of its food sealing products to FDA 177.2600 standards.
Food safety is a hot issue, and with all the recent public scares, one that is not likely to fade any time soon. One key area is the migration of contaminants from co...More...
|
| 20/05/2010 - Nation's NEW favourite thread lock is available from ERIKS |
Henkel has carried out research with thousands of customers worldwide in order to update its iconic Loctite 243 and 270 thread lock products. The results highlighted some areas of possible improvement, which the company's research department turned into two completely new formulas.
The results of the survey were passed to...More...
|
| 11/01/2010 - Fenner QuickDrive Inverter Range Expanded |
The Fenner QuickDrive (QD) range of inverters is being expanded with the addition of an IP66 rated QD:E model. The IP66 unit is available from 0.37kW to 7.5kW (110-440V) and is specifically designed with a smooth crevice free shape to reduce the opportunities for the build-up of debris. The Fenner QD:E (E for E...More...
|