Agricultural Chain | Agricultural Chain in todays world of sophisticated agricultural and processing equipment, the name Renold is the guarantee of outstanding quality and reliability.
Engineering design detail and precision manufacturing techniques have earned Renold the ISO 9000 (BS 5750) quality assurance standards, resulting in a range of chains giving longer life under the most arduous conditions.
Renold chain are used on:- Combine Harvesters
- Vegetable Grading Conveyors
- Grain Elevators
- Round Balers
- Circular Bale Unrollers
- Back-Feed Hoppers
- Box Scrapers
- Fruit Packing Conveyors
|
| - However, with continually improving farming techniques and higher crop yields, Renold also offers a range of extra strength chains which are dimensionally identical to the standard range.
- Heat treatment techniques are used to greatly enhance the breaking load and these chains have been adopted as a standard by major combine harvester manufacturers.
|
| Being dimensionally the same as the standard chain, they are more cost effective by:- Directly replacing standard chain using existing sprockets
- Increased load handling capabilities
These same advantages can also be realised when using extra strength chains to replace both malleable iron and pressed steel detachable link pintle chains. |
|
| |
|